You are here: Advanced Topics > Motion Techniques > Torque Feedforward

Torque Feed-forward

The torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist feed-forwardThis describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment tells the controller what forces is required to move the axis in an arbitrary trajectory.

Here are the major features of torque feed-forward:

 

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™